Press Releases
New Mini PLCs from RS Components Save Wiring, Space, Power and Programming Time
Barth Elektronik STG-500 and STG-600 need no peripherals, and allow easy graphical programming
Hong Kong, 16 June 2015:
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has extended its automation and control portfolio with ultra-compact mini PLCs that require no peripheral components for autonomous operation, thereby helping to simplify wiring and assembly.
The Barth Elektronik STG-500 and STG-600 mini PLCs provide 10 I/Os and 19 I/Os respectively, comprising digital, analogue and PWM channels. A temperature sensor is also built in. The STG-500 measures 40mm x 40mm x 22mm and has a universal aluminium mounting plate, while the STG-600 has an ultra-flat 10mm-high housing and maximum dimensions of 93mm x 45mm x 15mm.
Both models have very low current consumption and a wide operating voltage range of 7V to 32V, making them ideal for use in 12V or 24V battery-powered applications. Built-in protection for all I/Os, high shock and vibration resistance, and IP20 sealing, ensure reliability in harsh environments.
In addition, graphical programming capability makes these mini PLCs convenient and easy to use. The downloadable miCon-L software suite meets the standards of the latest graphical programming languages, and also integrates simulation and test capabilities. The flexible programming option offers a variety of possibilities in industrial, automotive and maritime applications.
Users can start building applications quickly by ordering the STA-500 or STA-600 starter kit, which includes the mini PLC and all necessary cables and manuals.
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping around 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2015 had revenues of £1.27bn.
For more information, please visit the website at www.rs-online.com.
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com