Variacs

Variacs, also known as autotransformers, are specialized electrical transformers with just one winding. The winding serves as the transformer's main and secondary sides. Instead, typical transformers feature two coils that are not electrically coupled.

The one-winding resolution produces smaller, lighter, and less expensive transformers than conventional two-winding transformers. They also have a lower leakage reactance, a lower excitation current, and a higher VA rating for a given size and mass.

What Is A Variac Transformer?

A variac transformer is a variable autotransformer, also known as an autotransformer or auto var. It is an electromechanical device designed to vary the magnitude of its output voltage by varying the input and output currents ratio through its windings. The term "variac" comes from "variable alternating current."

Variac transformers are used to control the voltage of a power supply. They can be used to adjust the voltage supplied to equipment, or they can be used to test the effects of different voltages on equipment. Variacs are also useful for controlling high voltages safely.

There are several kinds from single-phase variac transformers up to 3-phase variac transformers. A 3-phase variac is a type of variable transformer that is designed to adjust the voltage of a 3-phase AC power supply. It can be used to control the speed of motors, the output of heaters, and the brightness of lighting systems, among other things.

Variac transformers are typically found in electronics labs and industrial settings where precise control over AC power is required. They can be used in applications such as testing electrical circuits, adjusting heating elements, and adjusting audio amplifiers.

How does A Variac Works and how to use

A Variac is an AC power supply with an adjustable output voltage. It uses a step-down transformer to reduce high-voltage AC mains (115/230V) to a lower voltage suitable for electronic devices. The high-voltage secondary winding of the transformer feeds power to your device through an outlet or plug.

You control the output voltage by rotating a knob on the unit's front panel. There are two different types of variacs: fixed and variable. Fixed variacs have one set output voltage, whereas variable variacs allow you to adjust their output voltage from 0V up to about 250V Like within limits set by its design specifications.

Uses Of Variac Transformer

Variacs and autotransformers are frequently used for:

  • Transmission and distribution of power - Variacs ensure that the voltage at the start of the power distribution line is the same as the voltage at the end.
  • Power conversions - Variacs can convert typical residential mains voltage bands used worldwide. For example, 200 volts to 250 or 100 volts to 130 volts.
  • Autotransformers are used in audio systems to adjust speakers to constant-voltage distribution and to meet impendence levels.

How To Choose A Variac

There are several ways to choose a variac. First, you need to determine your needs: do you want just one variac for all your equipment? Or one for each piece of equipment? How much power do you need? Do you want variable frequency or variable voltage?

If you plan on using more than one piece of gear that requires a variac, it's best to get one with multiple outlets so that all your gear can be plugged in at once. If you only have one type of piece of equipment that uses a variac, then it's easy - just get one with enough outlets for whatever equipment you plan on connecting up!

33 產品顯示為 Variacs

Results per page