Keyboard & Mouse Sets

What is a Keyboard?

A keyboard is defined as the set of typewriter-like keys that enables you to enter data into a computer or other devices. Computer keyboards are similar to electric-typewriter but contain additional typing keys. The standard layout of letters, numbers, and punctuation is known as QWERTY but can also come as AZERTY (French version) and QWERTZ.

Most keyboards have numbers, letters, symbols, arrows but some also have a numeric keypad, functions like volume control, buttons to power down or sleep the device. Keyboards also come wired or wireless.

What is a wireless connection compared to a wired connection?

You can connect your keyboard to the computer via Bluetooth or an RF receiver compare to wired keyboards which connect to the motherboard via USB cable, using USB Type A connector. Laptops have an integrated keyboard, however, these are classed as wired since that's how they are connected to the computer. When it comes to tablets or phones with touch interfaces, these do not require physical keyboards, but these are equipped with USB receptacles where you can attach your external keyboard.

What is a Computer Mouse?

Computer Mouse is an input device that is used alongside a personal computer. Moving a mouse along a flat surface can move the on-screen cursor to different items on the screen. These also come wired or wireless.

Difference between the wired & wireless computer mouse

The wired mouse is a big advantage for gamers. They do not present as many delays as wireless ones, and that is extremely important when precision is key. When using a wireless mouse you need to take into consideration nearby interference, which can make mouse movements choppy. That's why while playing games, a wired mouse is a better option. Another advantage of the wired mouse is a price. These tend to be cheaper than wireless and they don't need batteries either.

Wireless mouse is definitely more convenient. You do not need to worry about cables, they are portable and you can use them while in the meetings or presenting through the laptop. Wireless mouse can be used for your TV when you use it as a monitor and want to control it from the comfort of your sofa. It is easy to use when you want to use the same mouse on your laptop or computer whereas wired mice aren't easy to unplug and unravel to move.

Here at RS, we offer Keyboard and Mouse Sets tailored to your requirements.

49 Products showing for Keyboard & Mouse Sets

Results per page