Recently searched
      • Published 7 Mar 2023
      • Last Modified 7 May 2024
    • 13 min

    The Complete Guide to Screwdrivers - Different Types and Uses

    Our guide explains everything you need to know about screwdrivers and the different types available.

    Reviewed by Luqman Said Abdullah, Technical Support Engineer (January 2021)

    Screwdrivers are handheld tools specifically designed for inserting and removing screws. They come in a wide range of variations to match different types of screw drives. The drive or head of a screw features a cavity and protrusion that perfectly align with the tip of a screwdriver. By applying a turning force called torque, screws can be tightened or loosened in either a clockwise or counter-clockwise direction.

    What Uses and Applications Are Screwdrivers Best Suited for?

    The screwdriver is one of the most essential hand tools in any tool kit. There are many situations and professions where a screwdriver is integral to carrying out a specific task revolving around loosening or tightening fasteners.

    Some of the most common uses of screwdrivers include:

    • Electronics and electrical equipment
    • Opening mobile phones
    • Opening computers
    • Mechanical and industrial production
    • Woodworking and carpentry
    • Metalwork and fastening wood to metal
    • Flammable environments

    It should also be noted that some specific types of screwdriver are best suited to certain applications. For instance, the best electrician's screwdrivers will be insulated to protect the user. Conversely, Phillips screwdriver uses are more varied as these tools are suitable for a range of general-purpose applications.

    Types of Screwdrivers

    The different types of screwdrivers are typically determined by the drive tip shape which corresponds with the specific head type of a given screw. However, other screwdriver types are application-specific or are intended for particular industries.

    Some of the most common types of screwdrivers are detailed in the sections below.

    Phillips screwdriver tip

    Phillips Screwdriver

    Also known as cross-head screwdrivers, Phillips screwdrivers are one of the most common types. But what is a Phillips head screwdriver? These tools are designed to fit screws with Phillips heads, which have a cross-shaped recess - hence the alternative name of cross screwdriver. They were invented to cope with higher torsion.

    Shop now

    Torx screwdriver tip

    Torx or Star Screwdriver

    Known variously as star head screwdrivers, pointed screwdrivers, six-point screwdrivers, and torx screwdrivers, these versions are all the same type. Torx is the trademark for a type of screw head with a six-point star-shaped intrusion, hence the generic name star screwdriver. These exist to ensure even more torque can be applied, for example, in mechanical production.

    Shop now

    Insulated Screwdriver Tip

    Insulated Screwdrivers

    Also known as safety screwdrivers, insulated screwdrivers are important for taking safety precautions in potentially hazardous scenarios. They are constructed from non-conductive materials such as rubber. VDE screwdrivers are also designed with safety in mind. VDE is an internationally-accredited institution that tests tools to certify that they meet the necessary safety standards. These tools are ideal for electricians.

    Shop now

    Torque Screwdriver Tip

    Torque Screwdrivers

    Not to be confused with Torx, a screwdriver with torque is similar to a torque wrench. Both types are used to apply a specified torque, which is meant to be just enough but not too excessive. They are ideal for tightening screws sufficiently without breaking the material they are fastening and inversely tight enough so they do not fall out. A torquing screwdriver has a torque-limiting clutch that allows a limit on how much force is applied beyond a certain threshold.

    Flat head screwdriver tip

    Flathead Screwdriver

    The slot or flat-headed screwdriver is probably the most common form of hand tool. It has a flattened tip used for screws with a straight linear intrusion across the head. Flat blade screwdrivers are multi-purpose and can typically be used for a range of applications.

    Shop now

    Tri Wing screwdriver tip

    Tri-Wing Screwdriver

    These are used for specific devices such as consoles, mobile phones and cameras. They often feature quite small tips to enable use with smaller screws and components.

    Shop now

    Pozidriv screwdriver tip

    Pozidriv Screwdriver

    Pozidriv screwdrivers are essentially an upgraded version of Philips. They were designed to reduce cam-out, which is the process where a screwdriver slips out of the screw head when more torque is applied.

    Shop now

    Hex screwdriver tip

    Hex Screwdriver

    Allen keys or wrenches are more popular tools for loosening or tightening hex screws. However, hexagon screwdrivers exist to serve the same purpose and hex-head tools are often included in sets.

    Shop now

    Square screwdriver tip

    Square Screwdriver

    The square-headed screwdriver fits screws with a square-shaped recess. It was invented to reduce the cam-out issue of the slotted screws and therefore speed up the fastening process.

    Shop now

    Electric Screwdriver

    Electric Screwdrivers and Impact Drivers

    Electric or cordless screwdrivers are generally compact power tools that are good for various tasks such as assembling furniture or screwing into softwood or other similar materials. Impact drivers, on the other hand, are essentially a more heavy-duty screwdriver type, intended for tasks like tightening or loosening fasteners using sudden force to drive into or remove from harder, denser materials.

    Shop now

    Precision Screwdriver

    Precision Screwdrivers

    This type of screwdriver is used for very small devices where extremely small screws are used. An example of this would be precision work on watches and mobile phones.

    Other Screwdriver Types

    Triangle Screwdriver

    Tools featuring a triangle screwdriver head are less common, but they are ideal for certain applications. The triangular screwdriver head is beneficial as its design makes it more secure and tamper-proof than alternatives. These tools are often used with appliances, toys, and electronics.

    Magnetic Screwdrivers

    Screwdrivers with magnetic tips allow screws to be attracted by magnetic force. This reduces the risk of accidentally dropping them. Magnetised tools are useful for working on electronics where screws are small and can be easily dropped into hard-to-reach places.

    Ratchet Screwdrivers

    Ratcheting screwdrivers are a type of screwdrivers that have a built-in mechanism, allowing the application of force only in one direction while enabling free movement in the other direction. These hand tools function similarly to ratchet spanners.

    Screwdriver Brands

    Wera

    Click through to see our complete range of Wera screwdrivers and shop online today with RS.

    View Range

    Wiha

    With a vast range of Wiha screwdrivers, you are sure to find the right product for your needs when you shop with RS.

    View Range

    Bahco

    Browse our extensive range of Bahco screwdrivers and choose the best screwdriver for your application.

    View Range

    CK

    Explore the full range of screwdrivers available from CK and choose from a wide range of types and sizes.

    View Range

    Screwdriver Sizes

    Screwdrivers come in many different sizes. As well as the standard large, medium, and small screwdrivers, there are also stubby screwdrivers that are ideal for use in tight or confined spaces. The tip width and the length of both the blade and the overall tool are usually measured in millimetres (mm).

    You should note that some sorts and brands may offer different sizing options to others. For instance, there are four standard Phillips screwdriver sizes. These range from #0 to #4, where #0 is the smallest screwdriver.

    Some tools can also be classified by torx size. This is shown by the letter T followed by a number - for example, T10 screwdrivers. It ranges from miniature screwdrivers right up to T45 and beyond. This system can also be applied to screws, helping you choose the corresponding screwdriver type for a particular-sized screw.

    Parts of a Screwdriver

    The three main parts that constitute a screwdriver are as follows:

    • Handle
    • Shaft or shank
    • Drive tip or bit

    All three parts are made in a production process using machines to form the correct shape of material using an extruder and heat-treating it to achieve the desired tensile strength.

    Screwdriver handle image

    Screwdriver Handle

    Screwdriver handles are used for gripping and are generally shaped to prevent rolling on flat surfaces. They can also be ergonomically designed to improve comfort when gripping. The materials used in the manufacturing process have changed over time, and there is now also more variety in the tools intended for use in specific applications. Most commonly, the handles are ergonomic and made of a composite of hard plastic such as cellulose acetate and rubber. They can also be covered in a non-slip, soft material like thermoplastic rubber to improve grip.

    Screwdriver shaft image

    Shaft or Shank

    The shaft or shank is commonly made of strong steel to ensure that bending or twisting deformation does not occur when applying force. The shaft will be rounded or hexagonal to allow a spanner or wrench to be used to apply increased torque. The shaft generally has a different colour and material from the drive tip, which can be interchangeable.

    Screwdriver tip image

    Drive Tip or Bit

    The drive tip can be an integrated part of the shank if it is not detachable. Alternatively, it can be an interchangeable part known as a driver - similar to drill bits. These are designed for use with multi-bit tools. The tip may also be known as the screwdriver head.

    Sets of Screwdrivers

    Screwdriver Set

    Screwdriver sets are highly useful when it comes to having a variety of pieces in one place. For example, there are precision screwdriver sets for delicate electronic work, as well as more multi-purpose electrician screwdriver sets for professionals.

    Sets typically contain a variety of tools in a range of sizes. Depending on the set, this could include multiple different types or varying sized versions of the same tool. A popular example of this is torx screwdriver sets. The best set of screwdrivers will ultimately depend on your requirements so be sure to select the most suitable set for your task or industry.

    Shop Screwdriver Sets

    Product Spotlight

    Screwdrivers

    RS offers an extensive range of screwdrivers with types available to suit all requirements. Browse online now.

    View Range

    Factors to Consider When Selecting a Screwdriver

    With various types available, you may wonder how to choose the best set of screwdrivers for your task or project. When selecting a suitable screwdriver, consider the following factors:

    • Drive Type Compatibility: It is essential to match the screwdriver tip with the screw head type, such as Phillips, flathead, or torx, to prevent damage to both the screw and the tool.
    • Size and Length: The size and shaft length of the screwdriver should be appropriate for the job at hand, ensuring you can apply the necessary force and reach into the work area comfortably.
    • Handle Comfort and Grip: Choosing a screwdriver with an ergonomic handle that provides a secure grip can significantly improve control during use and reduce hand fatigue over extended periods.
    • Material and Durability: Choose screwdrivers made from durable materials, such as chrome vanadium steel, to ensure they can withstand the rigours of regular use without failing.
    • Insulation for Electrical Work: If you're working with electricity, select screwdrivers that are properly insulated to protect against electric shock and are suitable for the voltages you will encounter.
    • Magnetic Tip: A screwdriver with a magnetic tip can be particularly useful for holding screws in place, making it easier to work in tight or difficult-to-reach areas.

    Tips for Using Screwdrivers Effectively

    Upon choosing the right screwdriverto complete your task, it is important to understand the best practices to use it in the most effective way and for extending its lifespan further. Following are some of tips you can consider:

    Pre-drill Pilot Holes: Before driving a screw into wood or another material, pre-drilling a pilot hole can help guide the screw and prevent the material from splitting.

    Use the Correct Size: Always use a screwdriver that matches the size of the screw head to avoid slipping and damaging the screw.

    Apply Pressure Evenly: Make sure that the screwdriver is aligned with the screw and apply pressure evenly to maintain a firm grip and control over the tool.

    Leverage Your Wrist: For maximum torque, position your hand correctly on the screwdriver handle and use your wrist effectively to turn the screwdriver.

    Keep Them Organised: Properly storing your screwdrivers protects the tools from damage and keeps them organised and ready for use.

    Safety Precautions When Using Screwdrivers

    Apart from using the screwdriver effectively for your task, it is also crucial to consider your safety during use, particularly when you are using one during an industrial task, where safety is heavily prioritised to avoid the risk of injuries. Consider the following safety prior to picking up a screwdriver:

    • Wear Protective Gear: Always wear safety glasses to protect your eyes from flying debris, which can occur unexpectedly while working with screwdrivers.
    • Check for Damaged Tools: Before using a screwdriver, inspect it for signs of wear or damage to avoid accidents that can arise from using compromised tools.
    • Avoid Using Screwdrivers as Pry Bars: Screwdrivers should not be used as pry bars, as this misuse can lead to the tool breaking and potentially causing injury.
    • Keep Hands Clear: Position your hands and fingers away from the path of the screwdriver to prevent injuries in case the tool slips.
    • Work in a Well-lit Area: Adequate lighting is crucial to reduce the risk of accidents by ensuring you have a clear view of your work area.
    • Use Insulated Screwdrivers for Electrical Work: As mentioned above, when working on electrical tasks, use screwdrivers that are specifically designed and insulated for such work to protect yourself from electricshocks.

    FAQs

    Popular Screwdriver Brands

    Wera

    Wera

    A German brand, Wera stands out for its innovative screwdriver designs that prioritise user comfort and efficiency. Their tools feature unique handle shapes for optimal grip and torque transfer, along with colour coding for easy identification. Click through to see our complete range of Wera.

    View Range

    Wiha

    Wiha

    Wiha excels in producing precision screwdrivers crafted with premium materials for exceptional durability and performance. Their tools often feature ergonomic handles, precision tips, and innovative technologies like the SoftFinish grip. Explore a vast range of Wiha screwdrivers.

    View Range

    Bahco

    Bahco

    Bahco, hailing from Sweden, offers a range of screwdrivers known for their durability and efficiency. What sets Bahco apart is its focus on user comfort, with features like anti-roll handles and precision tips for optimal performance. Browse our extensive range of Bahco screwdrivers.

    View Range

    CK

    CK

    CK is recognised among professionals for its precision-engineered screwdrivers that blend functionality with ergonomic design. Its tools often feature anti-slip handles, magnetic tips, and high-quality materials for durability. Explore the full range of screwdrivers available from CK.

    View Range