Press Releases


RS Components introduces HOTcap™ high-operating temperature radial-leaded ceramic capacitors from Vishay

New K…H series of MLCCs defines new standard of performance and reliability for automotive applications

Hong Kong, 22 June 2016:

RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has announced availability of the new HOTcap™ series of radial-leaded multilayer ceramic capacitors (MLCCs) from Vishay that meets the extreme operating conditions demanded by automotive applications. The K…H series of high operating temperature, radial-leaded MLCCs offers unprecedented performance and reliability in a small package.

Utilising noble metal electrodes and high reliability multi-layer ceramic capacitor inserts, the K…H series features an unmatched maximum operating temperature of +175°C for all available ceramic dielectrics. These include: an ultra-stable C0G dielectric, which delivers a capacitance change of ±30ppm/K across the –55 to +175°C operating temperature range; and the X0U dielectric, which has a capacitance change of +22% to –56% across the temperature range.

Qualified according to AEC-Q200, the capacitors are highly suited for a range of automotive applications, including EMI filtering in various functional areas such as exhaust-gas and seat-position sensors; cable harnesses; and turbo-charger, throttle-valve and brake-system control.

Voltage ratings available are 50, 100 and 200V dc across both dielectrics. Capacitance values available range from 100pF up to 12,0000pF (50V dc) for the C0G dielectric devices, and from 47,000 up to 1,000,000pF (50V dc) for the X0U dielectric.

To accommodate extremely harsh operating conditions, the series is equipped with high-performance MLCC chips that have been manufactured using a wet-build process and feature noble metal electrodes, delivering high resistance to corrosion and oxidation. The capacitors offer straight or crimped leads with spacing of 2.5 and 5.0mm. The devices' lead wires measure 0.5 or 0.6mm and are constructed of 100% tinned copper-clad steel. The RoHS-compliant devices also offer a flame-retardant epoxy resin coating, in accordance with UL94V-0

A sample kit of the K…H MLCC series is also available, comprising a total of 24 capacitors with variants differing in voltage rating, capacitance value and dielectric. RS is among the first to stock the K…H capacitors across the EMEA and Asia Pacific regions.

About RS Components

RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping more than 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2016 had revenues of £1.29bn.

For more information, please visit the website at www.rs-online.com.

Further information is available via these links:

Twitter: @RSElectronics; @alliedelec; @designsparkRS

RS Components on Linkedin
http://www.linkedin.com/company/rs-components

Relevant Links:

Electrocomponents plc
www.electrocomponents.com

RS Components
www.rs-online.com

DesignSpark
http://www.designspark.com