Press Releases
Updated RF signal spectrum analyser from Tektronix now in stock at RS Components
Latest version of Tektronix’s USB-connected real-time spectrum analyser now in stock at RS, ideal for RF electronics design engineers in the factory or the field
Hong Kong, 4 August 2016:
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has introduced an addition to its extensive portfolio of high-performance cost-effective analysis tools with the latest and updated Tektronix USB real-time spectrum analyser, which offers improved functionality to electronics design engineers working with RF signals, and is ideal for field, factory or academic use.
The RSA306B, the latest RF signal analysis tool from Tektronix replacing the RSA306, adds new functionality and further benefits. The analyser’s wide frequency range from 9kHz to 6.2GHz covers the bandwidth from conducted EMI to the latest wireless LAN standard, allowing analysers to view data over the entire working spectrum.
Key features of the tool include: a minimum signal event duration of 100μs for 100% probability of intercept; and a real-time spectrum/spectrogram display over a 40MHz bandwidth, which minimises the time spent on transient discovery and interference hunting, allowing engineers an immediate insight into the toughest problems. Enhanced measurement options include mapping, modulation analysis, standards support and pulse measurements. Other specifications include a +20 to –160dBm measurement range and spurious-free dynamic range (SFDR) of 60dBc (typical).
Ready to connect to a PC via its USB3.0 interface, the analyser operates with the SignalVu-PC software. This provides 17 spectrum and signal analysis measurements as standard and is the same analysis software as used on Tektronix's high-performance signal analysers and oscilloscopes, providing users with measurement confidence and high flexibility while problem solving. Direct control of the RSA306B is provided via the API, which means that users can transfer data to other programs for further analysis; for example, also included is a MATLAB driver, which has support for Instrument Control Toolbox. Additionally, streaming capture to disk enables gapless recording of long-duration events to aid in troubleshooting and interference hunting.
The RSA306B performs a wide range of functions including radio emissions testing using quick, complete and time-saving EMI checks for pre-compliance and diagnostics. Troubleshooting can also be investigated using powerful debug tools such as DPX and Domain correlation. Bluetooth and WLAN testing and troubleshooting are provided using module support that speeds up testing for popular IoT wireless standards. Regulatory monitoring capability is also provided by the industry’s best open signal database, so users can see signal compliance at a glance.
The portable and lightweight device, measuring only 30.5 x 190.5 x 127mm and weighing only 560g, is compliant with Mil-STD-28800 Class 2 environmental, shock and vibration specifications, making it ideal for use in harsh conditions in problem areas, whether inside or outside and in either hot or cold environments.
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping more than 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2016 had revenues of £1.29bn.
For more information, please visit the website at www.rs-online.com.
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
RS WeChat ID: RS_Components_CN
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com