Press Releases
RS Components introduces new additions to the ISO-TECH range of high-quality hand-held digital storage oscilloscopes
Portable IDS-200 and IDS-300 two-channel hand-held digital storage oscilloscopes – exclusive to RS Components – are ideal for
electrical installation engineers and site maintainers
Hong Kong, 30 June 2016:
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has extended the ISO-TECH range of test and measurement equipment with high-tech hand-held two-channel Digital Storage Oscilloscopes (DSOs). Exclusive to RS Components, the latest additions to the range include the IDS-200 and IDS-300 hand-held DSOs, which are perfect for electrical installation engineers and site maintainers and are available at highly accessible prices.RS is significantly expanding its ISO-TECH test and measurement range, which now comprises more than 500 devices suitable for the full range of electronic and electrical applications. The new IDS-200 and IDS-300 series feature touchscreen capacitive-LCD technology, which enables fingertip control of the device. Using only one finger, a waveform can be moved and a line position can be triggered; and using two fingers allows the adjustment of voltage levels and time-division scales. The touchscreen technology also offers an intuitive menu that enables operations such as fingertip control over the location of measurement functions and anytime-anywhere saving and retrieving both diagrams and data.
The ISO-TECH IDS-200 and IDS-300 hand-held two-channel DSOs offer a maximum sample rate of 1-Gsample/s and are available in entry-level models – the IDS-207 70MHz, IDS-210 100MHz and IDS-220 200MHz, and advanced models – the IDS-307 70MHz, IDS-310 100MHz and IDS-320 200MHz. In addition, the IDS-200 models offer memory depth of 1Mpts per channel and a DMM count of 5000, whereas the IDS-300 models provide a memory depth of 5Mpts per channel, a DMM count of 50,000 and temperature measurement.
These lightweight high-functionality devices weigh only 1.5kg and are robust and easily portable around any worksite, providing easy measurement and fast data analysis. They are supplied with everything needed to get up and running as soon as possible, including: a 150MHz probe for use with IDS-207/307/210/310 or a 250MHz probe (for use with IDS-220/320); test lead; power cord; soft carrying case; soft carrying bag; AC-DC adapter; wrist strap, Quick Start guide; and CD user manual.
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping more than 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2016 had revenues of £1.29bn.
For more information, please visit the website at www.rs-online.com.
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com