Press Releases
New SIMATIC S7-1200 CPUs With Upgraded Firmware Recommended for New Designs, Now Available From RS Components
V4.1 firmware makes popular PLC platform faster, more flexible, and failsafe-ready
Hong Kong, 17 June 2015:
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, is now shipping the latest in the popular Siemens SIMATIC S7-1200 CPU series, featuring upgraded firmware V4.1 that introduces performance improvements, extra features, and support for forthcoming failsafe CPUs.
The new firmware has improved instruction processing for faster execution of PLC programs, while increased work memory makes extra resources available for program and user data.
New features include enhanced motion capabilities such as position control and support for analogue or PROFIdrive drives. A PID control block allows temperature control in active heating or cooling systems, as well as interval measurements using high-speed counters. In addition, a built-in station web server allows flexible access via IP address. There is also dynamic copy protection, support for shared I-Device allowing connection of multiple controllers and fast data exchange, and enhanced configuration handling that allows modules to be specified and left unconnected without triggering alarms.
The firmware also introduces support for the forthcoming failsafe S7-1200 CPUs and signal modules (SM) for implementing safety-related appliances.
The latest S7-1200 FW4.1 CPUs, available now at RS Components, are recommended for new designs. 13 part numbers offer versatile configurations of analogue and 24V digital inputs and outputs. Version 4.1 firmware is also available to download for existing S7-1200 CPUs.
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping around 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2015 had revenues of £1.27bn.
For more information, please visit the website at www.rs-online.com.
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com