Recently searched
      • Published 10 Feb 2023
      • Last Modified 14 May 2024
    • 10 min

    Silicone Sealants - A Complete Buying Guide

    What are the different types of silicone sealants and where can they be used? Find out more in our handy guide.

    What is Silicone Sealant?

    Silicone sealant is a versatile silicone adhesive often employed to forge watertight or airtight seals at the interface of two surfaces. Also referred to as silicone glue, this sealant is one among many types of sealing solutions, including a variety of caulks and mastics.

    With an initial consistency akin to a liquid or gel, silicone sealant undergoes a curing process that solidifies it into a durable, flexible form akin to solid silicone rubber. This curing occurs under specific temperature and humidity conditions over time.

    Typically available in easy-to-use squeeze tubes for manual application, silicone sealant is also offered in larger, rigid cartridges. These are designed for use with a sealant gun or dispensing syringe, which can help achieve a cleaner application.

    In this guide, we will provide a comprehensive overview of silicone sealant uses, including the types ideal for creating strong, waterproof seals. We will also include practical advice on the application and address common queries, such as how to remove silicone sealant from various surfaces.

    Uses of Silicone Sealant

    As noted above, one of the most common uses of silicone sealant is to create a waterproof, airtight join between two surfaces or angles. More often than not, this will be in a well-used location that requires the creation of a durable yet somewhat elastic seal in order to keep out unwanted air or moisture.

    Silicone sealants are often chosen over other kinds of sealants,adhesives and caulks because of their improved flexibility and durability. Once cured, they create a tough yet slightly elastic bond that holds its shape extremely well over time and remains relatively inert at both higher and lower extremes of temperature.

    These qualities tend to make silicone the ideal material choice for creating hardwearing, long-lasting seals and joins in frequently used or particularly harshly exposed areas and environments. The rubbery nature of dried silicone seals makes them especially good at providing cushioning between surfaces that are liable to move, either because of mechanical forces or through expansion or contraction caused by moisture and temperature variations.

    In general, uses of silicone sealants tend to fall into one of four main categories. These are home repairs and maintenance, construction sealing and adhesion, glass and plastic bonding in craft or pet projects (including terrarium and aquarium seals), and manufacturing or production uses across a wide range of products, including electronics, appliances and automobiles.

    Typical examples of locations where sealing with silicone glues is especially commonplace might include:

    • Window seals
    • Door seals
    • Shower or bath sealing and edging
    • Cooker seals
    • Fridge seals
    • Plumbing joints
    • Electrical repair
    • Wire entry seals
    • Junction protection

    Besides its physical material properties, there are many other good reasons why professionals and DIY hobbyists alike often choose silicone sealants over the many other types of adhesives and mastics on offer (such as polyurethane sealants and acrylic adhesives).

    For one thing, the reliability and stability of a silicone seal once cured is particularly impressive. They’re also very easy to use, enabling the user to create a waterproof join with minimal effort, thanks to their quick and simple application. The curing process is fuss-free, requiring little further input from the user except to wait for the liquid gel to set itself in place.

    Silicone sealants are often weather-proof, and different sorts of products can withstand a wide range of demanding conditions, both indoors and outdoors. They’re chemically unreactive, do not promote mould growth, and they bond effortlessly to many other different surfaces and other materials thanks to the inclusion of specially formulated adhesive compounds.

    All of this means that you can typically expect to achieve a robust, reliable and long-lasting silicone seal that should require very little maintenance in order to stay in great condition for a prolonged period of time.

    How to Use Silicone Sealant

    Silicone Sealant

    If you’re planning on learning how to use silicone sealant or wondering how to get the perfect silicone seal (either via manual application or using a caulking gun), there are a number of handy tips and techniques to bear in mind.

    Silicone Sealant

    First and foremost is the importance of choosing the right product for the specific application and install environment that you are working on. We’ll cover the various different types of silicone sealants in the next section of this guide.

    Silicone Sealant

    Secondly, it’s worth taking the time to familiarise yourself with basic application techniques in order to neatly create joins or beads with silicone products. The correct application can go a long way towards ensuring the sealant remains as effective as possible.

    Different Silicone Sealant Types

    Silicone sealants come in a range of different colours, such as black, grey, white and clear. They typically come in a cartridge or tube, and many have a nozzle for precise bead application. There are squeeze tubes which are used for application by hand, or rigid tubes for use with a sealant gun.

    Silicone sealants typically fall into one of two main categories, namely neutral cure and acid cure (or acetoxy) variants. The latter is great for non-porous surfaces like glazed tiles and glass, but you’ll probably want to stick to neutral-cure silicone for working with wood or scratchable plastics and metals, as the acidic variants can cause corrosion or damage when applied directly to less suitable materials.

    High-modulus sealants tend to cure faster and harder and emit a slight vinegary smell as they cure. Most acetoxy silicone sealants are high modulus, while most neutral cure varieties will typically be low modulus, with very little odour and a slightly slower curing process resulting in a more flexible, elastic seal.

    The majority of silicone sealant products tend to be multi-purpose. They can normally be used in a wide variety of general applications and are suitable for creating bonds with many surface materials. Sanitary silicone sealants are best for wet applications, for example in bathrooms, because they are more stubbornly resistant against mould and mildew growth.

    A key aspect that you should always consider when purchasing caulks and mastics is whether or not a given product is explicitly listed as being an indoor/outdoor silicone sealant. You should also bear in mind any specific operating temperature ranges included in the product instructions.

    While silicone sealant broadly tends to be a strong performer in both warmer and colder climates (especially once cured), the presence of excessive heat or cold during the actual application process itself can sometimes affect a silicone adhesive’s ability to cure evenly and neatly around a join. This is a particularly important consideration for any seals that need to remain completely waterproof or airtight.

    Many different types of mastics, glues and caulks are advertised as having chemical formulas that support specific usage scenarios. Popular examples are waterproof silicone sealant, quick-drying silicone sealant, and high elongation variants. Other labels and features you might see on sealant packaging or in manufacturer guidelines could include the following:

    • Flexible
    • Fungus/mildew resistant silicone
    • High elasticity
    • High strength
    • High temperature
    • Low shrinkage
    • Low modulus
    • Low odour
    • Non-corrosive
    • Non-flammable
    • Tack-free

    Silicone Sealant Colours

    Silicone sealants are sold in numerous colours. However, the most popular options by far are white and clear silicone sealant varieties.

    With that being said, more and more colours of silicone have been made available as the range of vibrant colours and shades used in many common fittings and fixtures has broadened over time. It’s now relatively easy to find copper, greyred, cream, and black silicone sealants all being sold by a single brand or supplier.

    In cases where a more neutral or versatile look is required, translucent or transparent silicone sealant is also an option. This is particularly well-suited to glass bonds and is ideal for use on multi-coloured or patterned appliances and fixtures.

    Transparent Silicone Sealants

    Frequently Asked Questions (FAQs)

    Popular Silicone Sealant Brands

    Dow Corning

    Dow Corning

    Dow Corning provides a comprehensive range of silicone sealants tailored to diverse sealing requirements. Explore their assortment to find the perfect product for your needs.

    Shop Now

    Bostik

    Bostik

    Discover a wide array of Bostik silicone sealant products suitable for various applications. Explore their selection online and find the right sealant for your project.

    Shop Now

    Geocel

    Geocel

    Geocel offers silicone sealants designed to meet the highest standards of performance and reliability. Browse their range available online at RS Components and shop today.

    Shop Now

    RS PRO

    RS PRO

    Explore the full range of RS Pro silicone sealant products, meticulously crafted to ensure quality and durability. Find the ideal sealant for your project requirements.

    Shop Now